Solid Edge Geometry Type Library
IsVoid Property
Collapse All
Expand All
Solid Edge Geometry Type Library
>
CurvePath Object
: IsVoid Property
Description
Specifies whether or not the referenced Shell encloses material.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsVoid As Boolean
Remarks
IsVoid returns True if the material is on the outside of the CurvePath or Shell.
See Also
CurvePath Object
|
CurvePath Members