Solid Edge Geometry Type Library
Add Method
Specifies the Edge, Face, or Vertex to be added to the collection.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Sub Add( _
   ByVal Item As Object _
) 
Parameters
Item
Specifies the Edge, Face, or Vertex to be added to the collection.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As SolidEdgeGeometry.Body
    Dim objEdges As Object
    Dim objEdgesCol As Object
    Const TESTFILE = "T:\vbtests\testcases\freeform.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    ' Close active document if any
    Call objDoc.Close
    ' Open a testcase file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the body object of the model
    Set objBody = objDoc.Models(1).Body
    'Create an userdefined EdgeCollection object
    Set objEdgesCol = objBody.CreateCollection(Type:=seEdgeCollection)
    ' Get the edges of the body object
    Set objEdges = objBody.Edges(EdgeType:=igQueryAll)
    ' Add few items to EdgeCollection
    Call objEdgesCol.Add(objEdges(1))
    Call objEdgesCol.Add(objEdges(3))
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objEdges = Nothing
    Set objEdgesCol = Nothing
End Sub
See Also

Edges Collection  | Edges Members