Solid Edge Geometry Type Library
GeometryForm Property
Description
Specifies the geometry form of the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property GeometryForm As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBody As SolidEdgeGeometry.Body
    Dim objEdge As SolidEdgeGeometry.Edge
    Dim lngGeomForm As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' creating the base feature
    If CreateModel(objDoc) <> "" Then
        MsgBox "Error creating the model"
        Exit Sub
    End If
    ' getting the body object of the model
    Set objBody = objDoc.Models(1).Body
    'getting an edge from the collection of edges of the body
    Set objEdge = objBody.Edges(EdgeType:=igQueryAll).Item(1)
    ' getting the geometry form of the edge
    lngGeomForm = objEdge.GeometryForm
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objEdge = Nothing
End Sub
See Also

Edge Object  | Edge Members