Solid Edge Geometry Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objEdges As Object
    Dim objGeom As Object
    Dim objEllpEdge As solidedgegeometry.Edge
    Dim objEllipse As solidedgegeometry.Ellipse
    Dim objApplicn As SolidEdgeframework.Application
    Const TESTFILE = "T:\vbtests\testcases\Curve3d.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Open the TestFile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the Model object
    Set objBody = objDoc.Models(1).Body
    ' Get Edges Collection object
    Set objEdges = objBody.Edges(EdgeType:=igQueryEllipse)
    ' Get an Elliptical Edge
    Set objEllpEdge = objEdges(1)
    ' Get the Elliptical Curve
    Set objEllipse = objEllpEdge.Geometry
    ' Get the Application property
    Set objApplicn = objEllipse.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objApplicn = Nothing
    Set objEllpEdge = Nothing
    Set objEdges = Nothing
    Set objEllipse = Nothing
End Sub
See Also

Ellipse Object  | Ellipse Members