Solid Edge Geometry Type Library
GetCenterPoint Method
Returns the coordinates of the point that is the center of the referenced object.
Description
Returns the point that is the center of the referenced object.
Syntax
Visual Basic
Public Sub GetCenterPoint( _
   ByRef CenterPoint() As Double _
) 
Parameters
CenterPoint
Returns the coordinates of the point that is the center of the referenced object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objEdges As Object
    Dim objGeom As Object
    Dim objEllpEdge As solidedgegeometry.Edge
    Dim objEllipse As solidedgegeometry.Ellipse
    Const TESTFILE = "T:\vbtests\testcases\Curve3d.par"
    Dim dblCenPt() As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Open the TestFile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the Model object
    Set objBody = objDoc.Models(1).Body
    ' Get Edges Collection object
    Set objEdges = objBody.Edges(EdgeType:=igQueryEllipse)
    ' Get an Elliptical Edge
    Set objEllpEdge = objEdges(1)
    ' Get the Elliptical Curve
    Set objEllipse = objEllpEdge.Geometry
    ' Get the CenterPoint
    Call objEllipse.GetCenterPoint(CenterPoint:=dblCenPt())
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objEllpEdge = Nothing
    Set objEdges = Nothing
    Set objEllipse = Nothing
End Sub
See Also

Ellipse Object  | Ellipse Members