Solid Edge Geometry Type Library
GetMajorAxis Method
Returns the vector coordinates.
Description
Returns the coordinates of the major axis vector for the referenced object.
Syntax
Visual Basic
Public Sub GetMajorAxis( _
   ByRef MajorAxis() As Double _
) 
Parameters
MajorAxis
Returns the vector coordinates.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objEdges As Object
    Dim objGeom As Object
    Dim objEllpEdge As solidedgegeometry.Edge
    Dim objEllipse As solidedgegeometry.Ellipse
    Const TESTFILE = "T:\vbtests\testcases\Curve3d.par"
    Dim dblMajAxis() As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Open the TestFile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the Model object
    Set objBody = objDoc.Models(1).Body
    ' Get Edges Collection object
    Set objEdges = objBody.Edges(EdgeType:=igQueryEllipse)
    ' Get an Elliptical Edge
    Set objEllpEdge = objEdges(1)
    ' Get the Elliptical Curve
    Set objEllipse = objEllpEdge.Geometry
    ' Get the MajorAxis
    Call objEllipse.GetMajorAxis(MajorAxis:=dblMajAxis())
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objEllpEdge = Nothing
    Set objEdges = Nothing
    Set objEllipse = Nothing
End Sub
See Also

Ellipse Object  | Ellipse Members