Solid Edge Geometry Type Library
EdgeUses Property
Description
Returns a collection of EdgeUse objects for the referenced Loop.
Property type
Read-only property
Syntax
Visual Basic
Public Property EdgeUses As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objFaces As Object
    Dim objLoops As Object
    Dim objLEdgeUses As Object
    Const TESTFILE = "T:\vbtests\testcases\freeform.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' opening the test case file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' geting the body object from the model
    Set objBody = objDoc.Models(1).Body
    ' getting the collection of faces from the body object
    Set objFaces = objBody.Faces(facetype:=igQueryAll)
    ' getting a loop from the collection of loops for a particular face
    Set objLoops = objFaces(1).Loops
    ' getting the collection of edgeuses for a particular loop
    Set objLEdgeUses = objLoops(2).EdgeUses
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objFaces = Nothing
    Set objLoops = Nothing
    Set objLEdgeUses = Nothing
End Sub
See Also

Loop Object  | Loop Members