Solid Edge Geometry Type Library
ParamBSplineCurve Object
Members
Collapse All
Expand All
Solid Edge Geometry Type Library
: ParamBSplineCurve Object
Description
Describes the 2-D B-Spline curve.
Remarks
The methods on this object provide access to the BSpline curve geometry that fully describes the curve. Special properties of the curve are also returned by the methods.
See Also
ParamBSplineCurve Members