Solid Edge Geometry Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objFace As Object
    Dim ObjSphere As solidedgegeometry.Sphere
    Dim objSphereApp As SolidEdgeFramework.Application
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create base feature
    If CreateModel(objDoc) <> "" Then
        MsgBox "Error creating the model"
        Exit Sub
    End If
    'Get a handle to spherical face object
    Set objFace = objDoc.Models(1).Body.Faces(FaceType:=igQuerySphere)
    'Get handle to the Sphere object
    Set ObjSphere = objFace(1).Geometry
    'Get the Application object from Sphere
    Set objSphereApp = ObjSphere.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objFace = Nothing
    Set ObjSphere = Nothing
    Set objSphereApp = Nothing
End Sub
See Also

Sphere Object  | Sphere Members