Solid Edge Geometry Type Library
GetAxisVector Method
Returns the unit vector that defines the axis of a Cone or Cylinder object, the unit vector that is perpendicular to the circle of a Circle or Ellipse object , or the unit vector that is perpendicular to the major circle of a Torus object.
Description
Returns the unit vector that defines the axis of the referenced object.
Syntax
Visual Basic
Public Sub GetAxisVector( _
   ByRef AxisVector() As Double _
) 
Parameters
AxisVector
Returns the unit vector that defines the axis of a Cone or Cylinder object, the unit vector that is perpendicular to the circle of a Circle or Ellipse object , or the unit vector that is perpendicular to the major circle of a Torus object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objTorus As SolidEdgeGeometry.Torus
    Dim dblAxisVector() As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' creating the model object (a torus)
    If (CreateModel(objDoc) <> "") Then
        MsgBox "Error creating the model"
        Exit Sub
    End If
    ' getting the torus geometry object
    Set objTorus = objDoc.Models(1).Body.Shells(1).Faces(1).Geometry
    ' getting the axis vector of the torus
    Call objTorus.GetAxisVector(AxisVector:=dblAxisVector)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objTorus = Nothing
End Sub
See Also

Torus Object  | Torus Members