Solid Edge Geometry Type Library
GetCenterPoint Method
Returns the coordinates of the point that is the center of the referenced object.
Description
Returns the point that is the center of the referenced object.
Syntax
Visual Basic
Public Sub GetCenterPoint( _
   ByRef CenterPoint() As Double _
) 
Parameters
CenterPoint
Returns the coordinates of the point that is the center of the referenced object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objTorus As SolidEdgeGeometry.Torus
    Dim dblCenterPoint() As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' creating the model object (a torus)
    If (CreateModel(objDoc) <> "") Then
        MsgBox "Error creating the model"
        Exit Sub
    End If
    ' getting the torus geometry object
    Set objTorus = objDoc.Models(1).Body.Shells(1).Faces(1).Geometry
    ' getting the center point of the torus
    Call objTorus.GetCenterPoint(CenterPoint:=dblCenterPoint)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objTorus = Nothing
End Sub
See Also

Torus Object  | Torus Members