Solid Edge Geometry Type Library
Type Property
Description
Returns a member of the GNTTypePropertyConstants set to indicate the type of the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Type As GNTTypePropertyConstants
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objTorus As SolidEdgeGeometry.Torus
    Dim lngType As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' creating the model object (a torus)
    If (CreateModel(objDoc) <> "") Then
        MsgBox "Error creating the model"
        Exit Sub
    End If
    ' getting the torus geometry object
    Set objTorus = objDoc.Models(1).Body.Shells(1).Faces(1).Geometry
    ' getting the type of the geometry object
    lngType = objTorus.Type
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objTorus = Nothing
End Sub
See Also

Torus Object  | Torus Members