Solid Edge Geometry Type Library
GetPointData Method
Returns the coordinates of the point.
Description
Returns the point data for the referenced object.
Syntax
Visual Basic
Public Sub GetPointData( _
   ByRef Point() As Double _
) 
Parameters
Point
Returns the coordinates of the point.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objVertex1 As solidedgegeometry.Vertex
    Dim objFaces As Object
    Const TESTFILE = "T:\vbtests\testcases\Vertices.par"
    Dim dblPtData(1 To 3) As Double
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Open the TestFile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the Model object
    Set objBody = objDoc.Models(1).Body
    ' Get the Faces collection
    Set objFaces = objBody.Faces(FaceType:=igQueryAll)
    ' Get a Vertex
    Set objVertex1 = objFaces(1).Vertices(1)
    ' Get the PointData of Vertex
    Call objVertex1.GetPointData(Point:=dblPtData)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objFaces = Nothing
    Set objVertex1 = Nothing
    Set objBody = Nothing
End Sub
See Also

Vertex Object  | Vertex Members