Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
CrossSectionType | The shape of the cross section of a Bead. Circular, U shaped, or V shaped. |
DieRadius | The radius of the rounding applied to the die side of the feature. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
EndCondition | The end treatment applied to an open profile Bead. Formed, Lanced, or Punched |
EndPunchWidth | The width of a punched end Bead. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
FormRadius | The radius of a Circular or V shaped Bead. |
Height | The height of the Bead. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
ModelingModeType | |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Profile | Sets and returns the Profile object used to construct the referenced feature object. |
PunchRadius | The radius of the rounding applied to the punch side of the feature. |
RoundingOption | Whether or not to apply rounding to the Bead feature. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Side | The side of offset of the Bead with respect to the Plate on which it resides. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
TaperAngle | The angle of the sides of a U shaped or V shaped Bead. |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |
Width | The width of a U shaped Bead. |