Solid Edge Part Type Library : Blend Object |
![]() | Deletes the referenced object. |
![]() | Returns the feature style. |
![]() | Returns the high and low range values for the referenced object. |
![]() | Inserts the referenced object in front of or behind another feature. |
![]() | Sets the feature style. |
![]() | Returns the active application object. |
![]() | Returns the AttributeSets collection object for the referenced object. |
![]() | |
![]() | |
![]() | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
![]() | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
![]() | Returns a collection of faces that are intersected by a specified vector. |
![]() | Returns True if a specified Attribute Set exists on the referenced object. |
![]() | Returns the modeling mode of the referenced object. |
![]() | Returns the name of the referenced object. |
![]() | Returns the parent object for the referenced object. |
![]() | |
![]() | Specifies the type of the object being referenced. |
![]() | Specifies whether or not the referenced object is displayed to the screen. |