Solid Edge Part Type Library
Name Property
Description
Returns the name of the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Name As String
Remarks
All objects have names that are unique within the scope of their parent.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objFeatures As SolidEdgePart.Features
    Dim objBodyFt As SolidEdgePart.BodyFeature
    Const TESTFILE = "T:\vbtests\testcases\BodyFtr.x_t"
    Dim strName As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Open the TestFile
    Set objDoc = objApp.Documents.OpenWithTemplate(TESTFILE, "Normal.par")
    ' Get the Features collection object
    Set objFeatures = objDoc.Models(1).Features
    Set objBodyFt = objFeatures.Item(1)
    If objBodyFt.Type <> igBodyFeatureObject Then
        MsgBox ("Not a BodyFeature object")
    End If
    ' Get the Name property
    strName = objBodyFt.Name
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objFeatures = Nothing
    Set objBodyFt = Nothing
End Sub
See Also

BodyFeature Object  | BodyFeature Members