The Chamfer object defines a chamfer feature along the edge of a solid. The orientation of the chamfer relative to the faces can be at a specified angle and distance from the common edge, or it can be defined as two specified distances from the common edge. A Chamfer object cannot exist alone; it can only be material removed at the common edge of two faces of an existing part.