| Solid Edge Part Type Library : Constraints Collection |
Add | |
AddHorizontalVertical | Make a planar face Horizontal/Vertical. |
AddHorizontalVerticalAlignment | Create Horizontal/Vertical relation between two key points. |
AddOffsetEx | Creates an Offset relation between source and target faces and optionally updates the value. |
Item |
Application | Returns the active application object. |
Count | Returns the number of objects in the referenced collection. |
Parent | Returns the parent object for the referenced object. |