| Solid Edge Part Type Library : ContourFlange Object |
Delete | Deletes the referenced object. |
GetDimensions | Returns the Dimensions collection object for the referenced object. |
GetExtentKeyPoint | |
GetProfiles | Returns the profiles associated with the referenced feature object. |
GetStatusEx | Returns the status of the specified object. |
GetStyle | Returns the feature style. |
Range | Returns the high and low range values for the referenced object. |
Reorder | Inserts the referenced object in front of or behind another feature. |
RollToFeature | Rolls the referenced Model object back to a specified feature. |
SetExtentEdgeChain | |
SetExtentFinite | |
SetExtentToEndOfEdge | |
SetExtentToKeyPoint | |
SetProfiles | Sets the profiles associated with the referenced feature object. |
SetStyle | Sets the feature style. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BendRadius | Sets and returns the inside radius of the bend. |
BendReliefDepth | Sets and returns the depth of the bend relief for the specified object. |
BendReliefType | Sets and returns a constant that specifies the Bend relief type. |
BendReliefWidth | Sets and returns the width of the bend relief. |
ChainedEdges | |
CloseCornerDiameter | |
CloseCornerType | |
CornerReliefType | Property That Specifies The Corner Relief Type To Be Used |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
ExtendBendRelief | |
ExtentDistance | |
ExtentSide | Sets and returns the reference plane side for the referenced object. |
ExtentType | Sets and returns the extent type for the referenced object. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
MitreAngleAtEnd | |
MitreAngleAtStart | |
MitreBendEdgesLargerThanDefaultBendRadius | |
MitreCutType | |
MitrePosition | |
MitreSideAtEnd | |
MitreSideAtStart | |
MitreTypeAtEnd | |
MitreTypeAtStart | |
Name | Returns the name of the referenced object. |
NeutralFactor | Sets and returns the neutral factor applied to the bend. If the UseGlobalNeutralFactor property is True, the global neutral factor is associatively applied, and this local value is ignored. |
Parent | Returns the parent object for the referenced object. |
Profile | Sets and returns the Profile object used to construct the referenced feature object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |
UseGlobalBendRadius | Specifies whether or not the global bend radius is to be applied to the referenced object. |
UseGlobalBendReliefDepth | Specifies whether or not the global bend relief depth is to be applied to the referenced object. |
UseGlobalBendReliefWidth | Specifies whether or not the global bend relief depth is to be applied to the referenced object. |
UseGlobalNeutralFactor | Specifies whether or not the global neutral factor is to be applied to the referenced object. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |