| Solid Edge Part Type Library : ConvertPartToSM Object |
Delete | Deletes the referenced object. |
ExactRange | |
GetEdgesAndFaces | |
GetOverriddenBendParameters | |
GetOverriddenCloseCornerParameters | |
GetRipEdges | |
GetRipVertices | |
GetStatusEx | Returns the status of the specified object. |
GetStyle | Returns the feature style. |
OverrideBendParameters | |
OverrideCloseCornerParameters | |
Range | Returns the high and low range values for the referenced object. |
Reorder | Inserts the referenced object in front of or behind another feature. |
RollToFeature | Rolls the referenced Model object back to a specified feature. |
SetEdgesAndFaces | |
SetRipEdges | |
SetRipVertices | |
SetStyle | Sets the feature style. |
Angle | |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BendReliefDepth | |
BendReliefType | |
BendReliefWidth | |
CornerClosureType | |
CornerTreatmentDiameter | |
CornerTreatmentType | |
DisplayName | |
EdgebarName | |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
FlipClosureOrder | |
InnerBendRadius | |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
KeepParentBody | |
Name | Returns the name of the referenced object. |
NeutralFactor | |
OffsetValue | |
OverlapRatio | |
Parent | Returns the parent object for the referenced object. |
RemoveInternalLoops | |
RipGap | |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | |
ThickenDirection | |
Thickness | |
Type | Specifies the type of the object being referenced. |
UseGlobalBendRadius | |
UseGlobalBendReliefDepth | |
UseGlobalBendReliefWidth | |
UseGlobalNeutralFactor | |
Visible | Specifies whether or not the referenced object is displayed to the screen. |
Width |