Solid Edge Part Type Library
CopySurface Object
Members 
Description
Represents an occurrence of a CopySurface construction element.
Object Model
CopySurface ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionSuppressVariable ObjectApplication Object
Remarks
A CopySurface object is a surface created using the faces of any part or construction feature as input.
See Also

CopySurface Members