Solid Edge Part Type Library
Dimple Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method GetDimensionsReturns the Dimensions collection object for the referenced object.
Public Method GetProfilesReturns the profiles associated with the referenced feature object.
Public Method GetStatusExReturns the status of the specified object.
Public Method GetStyleReturns the feature style.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReorderInserts the referenced object in front of or behind another feature.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Method SetProfilesSets the profiles associated with the referenced feature object.
Public Method SetStyleSets the feature style.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DepthSets and returns the distance that the referenced object extends or removes material from a solid.
Public Property DepthSideSets and returns the material side for the referenced object.
Public Property DieRadiusSets and returns radius value for the top of the referenced feature.
Public Property DimensionTypeSets and returns the type of dimension for the referenced object.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property MaterialSideSets and returns the direction in which material was added to the referenced object.
Public Property ModelingModeType
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property ProfileSets and returns the Profile object used to construct the referenced feature object.
Public Property ProfileCornerRadiusSets and returns the radius of the corner rounds for the referenced object.
Public Property ProfileSideSets and returns the side of the profile to which material is added or removed.
Public Property PunchRadiusSets and returns the radius value at the bottom of the referenced feature.
Public Property RoundCornersSets and returns a value that specifies whether or not the corners of the referenced object are to be rounded.
Public Property RoundEdgesSets and returns a value that specifies whether or not the edges of the referenced object are to be rounded.
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TaperAngleSets and returns the taper angle for the referenced object.
Public Property TypeSpecifies the type of the object being referenced.
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

Dimple Object