| Solid Edge Part Type Library : EmbossFeature Object |
Delete | Deletes the Emboss Feature. |
Edit | Can send new values to feature and it will be edited accordingly. |
ExactRange | |
GetEmbossToolBodies | Get Emboss Bodies. |
GetStatusEx | Returns the status of the specified object. |
Range | Returns the high and low range values for the referenced object. |
Reorder | Inserts the referenced object in front of or behind another feature. |
RollToFeature | Rolls the referenced Model object back to a specified feature. |
SetEmbossToolBodies |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Clearance | |
DieRadius | |
DieRounding | |
DisplayName | |
EdgebarName | |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
EmbossTarget | |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
PunchSideRadius | |
PunchSideRounding | |
ShowDimensions | Controls the display of dimensions for the feature object. |
Side | |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | |
Thicken | |
Thickness | |
Type | Specifies the type of the object being referenced. |