Solid Edge Part Type Library
Add Method
Specifies the Face object on which the edges are to be extended.
Specifies the number of input Edge objects.
Specifies the Edge objects comprising the face to be extended.
Specifies the arc length distance by which the edge is to be moved on the surface.
Member of the ExtendSurfaceExtentTypeConstants constant set that specifies a linear or natural extension for the surface. For analytic faces (planes, cylinders, cones, spheres, and tori) the option must be set to igESNatural, or the feature will fail.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Function Add( _
   ByVal FaceDispatch As Object, _
   ByVal NumberOfInputEdges As Long, _
   ByRef EdgesArray() As Object, _
   ByVal ExtensionDistance As Double, _
   ByVal ExtensionType As ExtendSurfaceExtentTypeConstants _
) As ExtendSurface
Parameters
FaceDispatch
Specifies the Face object on which the edges are to be extended.
NumberOfInputEdges
Specifies the number of input Edge objects.
EdgesArray
Specifies the Edge objects comprising the face to be extended.
ExtensionDistance
Specifies the arc length distance by which the edge is to be moved on the surface.
ExtensionType
ValueDescription
igESConstantRadiusArc
igESLinear
igESLinearCurvatureContinuous
igESLinearTangentContinuous
igESNatural
igESReflective
Member of the ExtendSurfaceExtentTypeConstants constant set that specifies a linear or natural extension for the surface. For analytic faces (planes, cylinders, cones, spheres, and tori) the option must be set to igESNatural, or the feature will fail.
See Also

ExtendSurfaces Collection  | ExtendSurfaces Members