| Solid Edge Part Type Library : ExtrudedSurface Object |
ApplyDirection1Extent | Applies extent information for the first direction. |
ApplyDirection1Treatment | Applies draft angle and crown information for the first direction. |
ApplyDirection2Extent | Applies extent information for the second direction. |
ApplyDirection2Treatment | Applies draft angle and crown information for the second direction. |
Delete | Deletes the referenced object. |
DropParents | Removes associative connection with parents, so that it can not edited or recomputed. |
GetDimensions | Returns the Dimensions collection object for the referenced object. |
GetDirection1Extent | Returns extent information for the first direction. |
GetDirection1Treatment | Returns draft angle and crown information for the first direction. |
GetDirection2Extent | Returns extent information for the second direction. |
GetDirection2Treatment | Returns draft angle and crown information for the second direction. |
GetFromFaceOffsetData | Returns from face data. |
GetProfiles | Returns the profiles associated with the referenced feature object. |
GetStatusEx | Returns the status of the specified object. |
GetStyle | Returns the feature style. |
GetToFaceOffsetData | Returns to face data. |
Range | Returns the high and low range values for the referenced object. |
Reorder | Inserts the referenced object in front of or behind another feature. |
RollToFeature | Rolls the referenced Model object back to a specified feature. |
SetFromFaceOffsetData | Sets from face data. |
SetProfiles | Sets the profiles associated with the referenced feature object. |
SetStyle | Sets the feature style. |
SetToFaceOffsetData | Sets to face data. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
EndCapsStatus | Sets and returns the end caps status for the referenced object. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
ModelingModeType | Returns the modeling mode of the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Profile | Sets and returns the Profile object used to construct the referenced feature object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
SideFaces | Returns a collection of all the side faces for the referenced feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |