| Solid Edge Part Type Library : FaceMove Object |
Delete | Deletes the referenced object. |
ExactRange | This method sets the exact range parameters for the referenced object. |
GetDimensions | This method returns the dimensions for the referenced object. |
GetStatusEx | Returns the status of the specified object. |
Range | Returns the high and low range values for the referenced object. |
Reorder | Inserts the referenced object in front of or behind another feature. |
RollToFeature | Rolls the referenced Model object back to a specified feature. |
AlongOrReverseVector | |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
Distance | Sets and returns the constraint distance for the referenced object. |
EdgeAlongDirectionToMove | |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
FaceAlongNormalToMove | |
FaceMoveBlendType | |
FaceMoveType | |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
FacesToMove | |
FromPoint | |
InPlane | |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
OffsetAlongOrReverseVector | |
offsetDistance | |
Parent | Returns the parent object for the referenced object. |
Point1Of2PointVector | |
Point2Of2PointVector | |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
ToPoint | |
Type | Specifies the type of the object being referenced. |