| Solid Edge Part Type Library : FaceSet Object |
Delete | Deletes the referenced object. |
GetStatusEx | Returns the status of the specified object. |
GetStyle | Returns the feature style. |
Range | Returns the high and low range values for the referenced object. |
Reorder | Inserts the referenced object in front of or behind another feature. |
SetStyle | Sets the feature style. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DisplayName | |
EdgebarName | |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
ModelingModeType | |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Status | Returns the status of the specified object. |
SystemName | |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |