Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Description | |
DisplayName | This read-only String property returns the display name for the referenced object. |
DocumentName | Sets and returns the name of the full-path specification of the PartDocument name that contains the referenced DividedPart or FamilyMember object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
LiveRule | Turns a live rule on or off. |
MovePrecedence | Controls the move precedence. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Status | Returns the status of the specified object. |
SuppressedFeature | Returns the suppressed feature having a specified index of a part in a family. |
SuppressedFeatureCount | Returns the number of suppressed features in a family of parts. |
SuppressedRelationship | Returns the suppressed relationship having a specified index in a family. |
SuppressedRelationshipCount | Returns the number of suppressed relationships in a family of parts. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |
Value | Returns the name of the application, the value of a dimension, the value of a custom property, or the value of a variable. |
Variable | Returns a Variable object having a specified index for the referenced FamilyMember object. |
VariableCount | Returns the number of variables in a FamilyMember object. |