Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DieRadius | Sets and returns radius value for the top of the referenced feature. |
DisplayName | This read-only String property returns the display name for the referenced object. |
Distance | Sets and returns the constraint distance for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
FormedRadius | This read-write Double property sets and returns the formed radius value for gusset feature. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
MaterialSide | Sets and returns the direction in which material was added to the referenced object. |
Name | Returns the name of the referenced object. |
NumberOfOccurrences | Returns the number of occurrences. |
OccurrenceSpacing | This read-write Double property sets and returns the spacing between gusset occurrences in the sheet metal document. |
Parent | Returns the parent object for the referenced object. |
PatternType | Sets and returns the pattern to apply to the referenced Gusset object. |
Profile | Sets and returns the Profile object used to construct the referenced feature object. |
PunchRadius | Sets and returns the radius value at the bottom of the referenced feature. |
Rounding | This read-write Double property specifies whether or not rounding is applied to a gusset feature. |
Shape | This read-write Double property specifies the shape of the gusset in the sheet metal document. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
TaperAngle | Sets and returns the taper angle for the referenced object. |
ThicknessSide | Sets and returns the side of the profile on which the thickness of the feature object was added. |
Type | Specifies the type of the object being referenced. |
Width | Returns the width of the referenced object. |