Solid Edge Part Type Library
Holes Collection Members
Overview 
Public Methods
Public Method AddFiniteAdds a 3-D feature object to an object collection.
Public Method AddFromToAdds or removes material from a feature between specified surfaces or reference planes.
Public Method AddSyncCreates a Synchronous Hole feature in the model.
Public Method AddThroughAllAdds or removes material from a feature starting at a specified surface and extending through all surfaces in the feature.
Public Method AddThroughNextAdds or removes material from a feature starting at a specified surface and extending through the next closed intersection in the feature.
Public Method ItemThe items in a collection.
Public Method RecognizeAndCreateHoleGroupsRecognizes and Creates a Synchronous Hole feature in the model.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property CountReturns the number of objects in the referenced collection.
Public Property ParentReturns the parent object for the referenced object.
See Also

Holes Collection