Solid Edge Part Type Library
IntersectSurface Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method ExactRange
Public Method GetEdgesToExtend
Public Method GetExtendType
Public Method GetHealOption
Public Method GetStatusExReturns the status of the specified object.
Public Method GetStitchOption
Public Method GetStitchTolerance
Public Method PutEdgesToExtend
Public Method PutExtendType
Public Method PutHealOption
Public Method PutStitchOption
Public Method PutStitchTolerance
Public Method RangeReturns the high and low range values for the referenced object.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DisplayName
Public Property EdgebarName
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property ModelingModeType
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemName
Public Property TypeSpecifies the type of the object being referenced.
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

IntersectSurface Object