Solid Edge Part Type Library
NeutralFactor Property
Description
Sets and returns the neutral factor applied to the bend.
Property type
Read-write property
Syntax
Visual Basic
Public Property NeutralFactor As Double
Remarks
If the UseGlobalNeutralFactor property is True, the global neutral factor is associatively applied, and this local value is ignored.
See Also

Jog Object  | Jog Members