Solid Edge Part Type Library
StartpointMagnitude Property
Description
Sets and returns the direction and degree of influence of the StartpointEdge on the curvature of the curve at the startpoint.
Property type
Read-write property
Syntax
Visual Basic
Public Property StartpointMagnitude As Double
Remarks
This value is meaningful only if the StartpointEndCondition is seKeypointEndConditionTangent.
See Also

KeyPointCurve Object  | KeyPointCurve Members