Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BottomNote1 | Sets and returns the Bottom Note 1 text for the referenced object. |
BottomNote2 | Sets and returns the Bottom Note 2 text for the referenced object. |
BottomNote3 | Sets and returns the Bottom Note 3 text for the referenced object. |
BottomNoteAngle | |
BottomNoteCSize | |
BottomNoteDepth | |
BottomNoteZ | Sets and returns the Bottom Note Z text for the referenced object. |
BottomPosOffset | |
BottomTreatmentType | Sets and returns the treatment display style to use for the bottom treatment portion of the referenced object. |
BottomType | Sets and returns the bottom type for the referenced object. |
BottomTypeCompound | Sets and returns the top type compound for the referenced object. |
CenterType | Sets and returns the bottom type compound for the referenced object. |
CrossSectionArea | Returns the cross-sectional area of the referenced LabelModelWeld object. |
DashLine | Sets and returns the relative position of the dash lines for the referenced weld symbol object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
OffsetTopBottom | Specifies whether the top and bottom weld types are offset or aligned. |
Parent | Returns the parent object for the referenced object. |
Symmetrical | Specifies whether or not the referenced object is symmetrical. |
Tail | Specifies whether the less than symbol appears at the end of the breaklline. |
TailNote | Sets and returns the tail note text. |
TailNote2 | Sets and returns the tail note text for the referenced object. |
TopNote1 | Sets and returns the Top Note 1 text. |
TopNote2 | Sets and returns the Top Note 2 text. |
TopNote3 | Sets and returns the Top Note 3 text. |
TopNoteAngle | |
TopNoteCSize | |
TopNoteDepth | |
TopNoteZ | Sets and returns the Top Note Z text. |
TopPosOffset | |
TopTreatmentType | Sets and returns the display style to use for the top treatment portion of the referenced object. |
TopType | Sets and returns the top type for the referenced object. |
TopTypeCompound | Sets and returns the bottom type for the referenced object. |
WeldAllAround | Specifies whether or not the 'weld all around' display style is included in the referenced object. |
WeldInField | Specifies whether or not the 'weld in field' display style is included in the referenced object. |
ZSymbol | Specifies whether or not the Z weld symbol modifier is included in the referenced object. |