Solid Edge Part Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objProfArr(1 To 2) As SolidEdgePart.Profile
    Dim objModel As SolidEdgePart.Model
    Dim objExtProt As SolidEdgePart.ExtrudedProtrusion
    Dim objRelns1 As SolidEdgeFrameworkSupport.Relations2d
    Dim objTemp As Object
    Dim objEdges(1 To 4) As Object
    Dim objSideFace As Object
    Dim objCapFace As Object
    Dim objLips As SolidEdgePart.Lips
    Dim objLip As SolidEdgePart.Lip
    Dim objLipApp As SolidEdgeFramework.Application
    Dim lngStatus As Long
    Dim i As Integer
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    ' Draw the Profile
    Set objProfArr(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Set objLines = objProfArr(1).Lines2d
    Call objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.06, y2:=0)
    Call objLines.AddBy2Points(x1:=0.06, y1:=0, x2:=0.06, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0.06, y1:=0.06, x2:=0, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0, y1:=0.06, x2:=0, y2:=0)
    ' Relate the Lines to make the Profile closed
    Set objRelns1 = objProfArr(1).Relations2d
    Call objRelns1.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart)
    ' Check for the Profile Validity
    lngStatus = objProfArr(1).End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Profile not closed")
    End If
    ' Create the Base Protrusion Object
    Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
                                                             ProfileArray:=objProfArr, profileplaneSide:=igRight, _
                                                             ExtrusionDistance:=0.02)
    objProfArr(1).Visible = False
    ' Check the status of Base Feature
    If objModel.ExtrudedProtrusions(1).Status <> igFeatureOK Then
        MsgBox ("Error in the Creation of Base Protrusion Feature object")
    End If
    Set objExtProt = objModel.ExtrudedProtrusions(1)
    '*** Lip Creation
    'Get the Lips collection from the Model object
    Set objLips = objModel.Lips
    'Get the edges on which lip is to be created in to an array
    Set objTemp = objExtProt.BottomCap.Edges
    For i = 1 To objTemp.Count - 1
        Set objEdges(i) = objTemp(i)
    Next i
    'Get the face to be set as SideFace for the Lip
    Set objSideFace = objExtProt.SideFaces.Item(1)
    'Get the face to be set as CapFace for the Lip
    Set objCapFace = objExtProt.BottomCap
    'Create the Lip
    Set objLip = objLips.Add(Numberofedges:=3, Edges:=objEdges, SideFace:=objSideFace, _
                             CapFace:=objCapFace, Width:=0.01, Height:=0.005)
    'Validate the feature
    If objLip.Status <> igFeatureOK Then
        MsgBox "Add method of Lip feature failed"
    End If
    'Get the Application object from Lips object
    Set objLipApp = objLips.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLines = Nothing
    Set objProfArr(1) = Nothing
    Set objProfArr(2) = Nothing
    Set objModel = Nothing
    Set objExtProt = Nothing
    Set objRelns1 = Nothing
    Set objTemp = Nothing
    Set objEdges(1) = Nothing
    Set objEdges(2) = Nothing
    Set objEdges(3) = Nothing
    Set objEdges(4) = Nothing
    Set objSideFace = Nothing
    Set objCapFace = Nothing
    Set objLips = Nothing
    Set objLip = Nothing
    Set objLipApp = Nothing
End Sub
See Also

Lips Collection  | Lips Members