Solid Edge Part Type Library
Load Object Members
Overview 
Public Methods
Public Method DeleteDelete a perticular load object.
Public Method GetFlipGer current Flip condition of load.
Public Method GetGeometriesGet an array of geometry objects on which the load has been applied.
Public Method GetLoadDirectionGet X, Y, Z directions from a load object.
Public Method GetLoadOptionsGet various option parameter values from existing load.
Public Method GetLoadTypeGet type of a load object.
Public Method GetLoadValueGet value of a load object.
Public Method GetLoadValueAngAccelnGet value of angular acceleration load object.
Public Method GetThermalLoadOptionsGet various option parameter values from existing Thermal load.
Public Method SetFlipFlip load direction, towards/away from entity.
Public Method SetGeometriesSet edges/faces/vertices etc as geometry to apply load on.
Public Method SetLoadDirectionSet X, Y, Z directions for a load object.
Public Method SetLoadOptionsSet/modify parameters like load value, symbol spacing, symbol size of an existing load object.
Public Method SetLoadTypeSet type of a load object.
Public Method SetLoadValueSet value on a load object.
Public Method SetLoadValueAngAccelnSet value of angular acceleration load object.
Public Method SetThermalLoadOptionsSet/modify parameters like load value, symbol spacing, symbol size, ambient temperature, view factor etc of an existing Thermal load object.
See Also

Load Object  | Solid Edge ST3 - What's New