Solid Edge Part Type Library
Suppress Property
Description
Temporarily suppresses the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Suppress As Boolean
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfArr(1 To 3) As SolidEdgePart.Profile
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objRelns1 As SolidEdgeFrameworkSupport.Relations2d
    Dim objModel As SolidEdgePart.Model
    Dim objRefPln As SolidEdgePart.RefPlane
    Dim objProf1 As SolidEdgePart.Profile
    Dim objProf2 As SolidEdgePart.Profile
    Dim objExtCut1 As SolidEdgePart.ExtrudedCutout
    Dim objExtCut2 As SolidEdgePart.ExtrudedCutout
    Dim objPatPln As SolidEdgePart.RefPlane
    Dim objFtArr(1 To 3) As Object
    Dim objMirr1 As SolidEdgePart.MirrorCopy
    Dim objMirrCps As SolidEdgePart.MirrorCopies
    Dim lngStatus As Long
    Dim bSupp As Boolean
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Draw the Profile
    Set objProfArr(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Set objLines = objProfArr(1).Lines2d
    Call objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.06, y2:=0)
    Call objLines.AddBy2Points(x1:=0.06, y1:=0, x2:=0.06, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0.06, y1:=0.06, x2:=0, y2:=0.06)
    Call objLines.AddBy2Points(x1:=0, y1:=0.06, x2:=0, y2:=0)
    ' Relate the Lines to make the Profile closed
    Set objRelns1 = objProfArr(1).Relations2d
    Call objRelns1.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart)
    Call objRelns1.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart)
    ' Check for the Profile Validity
    lngStatus = objProfArr(1).End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Profile not closed")
    End If
    ' Create the Base Protrusion Object
    Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
                                                             ProfileArray:=objProfArr, profileplaneSide:=igRight, _
                                                             ExtrusionDistance:=0.02)
    objProfArr(1).Visible = False
    ' Check the status of Base Feature
    If objModel.ExtrudedProtrusions(1).Status <> igFeatureOK Then
        MsgBox ("Error in the Creation of Base Protrusion Feature object")
    End If
    ' Create 2 Extruded Cutouts to act as Features for Mirroring
    ' Create a Circular Profile
    Set objRefPln = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objDoc.RefPlanes(1), _
                                                           Distance:=0, NormalSide:=igRight)
    Set objProf1 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objRefPln)
    Call objProf1.Circles2d.AddByCenterRadius(x:=0.02, y:=0.02, Radius:=0.005)
    ' Check if the Profile is closed
    lngStatus = objProf1.End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Profile not closed")
    End If
    'Create the ExtrudedCutout feature
    Set objExtCut1 = objModel.ExtrudedCutouts.AddThroughAll(Profile:=objProf1, _
                                                            ProfileSide:=igLeft, profileplaneSide:= _
                                                            igRight)
    objProf1.Visible = False
    If objExtCut1.Status <> igFeatureOK Then
        MsgBox ("Error in the Creation of ExtrudedCutout object")
    End If
    ' Create a Circular Profile
    Set objRefPln = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objDoc.RefPlanes(1), _
                                                           Distance:=0, NormalSide:=igRight)
    Set objProf2 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objRefPln)
    Call objProf2.Circles2d.AddByCenterRadius(x:=0.02, y:=0.04, Radius:=0.005)
    ' Check if the Profile is closed
    lngStatus = objProf2.End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Profile not closed")
    End If
    'Create the ExtrudedCutout feature
    Set objExtCut2 = objModel.ExtrudedCutouts.AddThroughAll(Profile:=objProf2, _
                                                            ProfileSide:=igLeft, profileplaneSide:= _
                                                            igRight)
    objProf2.Visible = False
    If objExtCut2.Status <> igFeatureOK Then
        MsgBox ("Error in the creation of ExtrudedCutout object")
    End If

    ' Create the PatternPlane for the Mirror object
    Set objPatPln = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objDoc.RefPlanes(2), _
                                                           Distance:=0.03, NormalSide:=igRight)

    ' Create a FeatureArray
    Set objFtArr(1) = objExtCut1
    Set objFtArr(2) = objExtCut2
    ' Create the Mirror
    Set objMirrCps = objModel.MirrorCopies
    Set objMirr1 = objMirrCps.Add(PatternPlane:=objPatPln, NumberOfFeatures:=2, FeatureArray:=objFtArr)
    If objMirr1.Status <> igFeatureOK Then
        MsgBox ("Add method of MirrorCopies object failed")
    End If
    ' Get the Suppress Property
    bSupp = objMirr1.Suppress
    objMirr1.Suppress = Not bSupp
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfArr(1) = Nothing
    Set objProfArr(2) = Nothing
    Set objModel = Nothing
    Set objLines = Nothing
    Set objRelns1 = Nothing
    Set objExtCut1 = Nothing
    Set objExtCut2 = Nothing
    Set objRefPln = Nothing
    Set objProf2 = Nothing
    Set objProf1 = Nothing
    Set objMirr1 = Nothing
    Set objMirrCps = Nothing
    Set objPatPln = Nothing
    Set objFtArr(1) = Nothing
    Set objFtArr(2) = Nothing
End Sub
See Also

MirrorCopy Object  | MirrorCopy Members