Solid Edge Part Type Library
MountingBoss Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method ExactRangeThis method sets the exact range parameters for the referenced object.
Public Method GetDimensionsReturns the Dimensions collection object for the referenced object.
Public Method GetInputFeaturesReturns the input feature for the referenced feature.
Public Method GetNumberOfOccurrencesReturns the number of occurrences for the referenced pattern object.
Public Method GetStatusExReturns the status of the specified object.
Public Method GetStyleReturns the feature style.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReorderInserts the referenced object in front of or behind another feature.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Method SetStyleSets the feature style.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property BossDiameterSpecifies the diameter of the referenced MountingBoss object.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property DraftAngleSpecifies the draft angle.
Public Property DraftEnabledSpecifies whether draft is enabled.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property ModelingModeTypeReturns the modeling mode of the referenced object.
Public Property MountingHoleDepthSpecifies the depth of the mounting hole.
Public Property MountingHoleDiameterSpecifies the diameter of the mounting hole.
Public Property MountingHoleEnabledSpecifies whether mounting hole is enabled for the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property NumberInputFeaturesReturns the number of input features for the referenced feature.
Public Property NumberOfRibsSpecifies the number of ribs.
Public Property OccurrenceIndexReturns the index for the feature occurrence for the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property PatternPlaneReturns the PatternPlane for the referenced object.
Public Property ProfilePlaneSideSpecifies the profile plane side for the referenced object.
Public Property RibExtentSpecifies the distance the ribs protrude from the side of the referenced object.
Public Property RibGradeSpecifies the angle of the ribs relative to the top face of the referenced MountingBoss object.
Public Property RibOffsetSpecifies the distance the ribs are offset from the top surface.
Public Property RibsEnabledSpecifies whether ribs are enabled.
Public Property RibTaperSpecifies the angle of the ribs relative to the cylindrical body.
Public Property RibThicknessSpecifies the thickness of the ribs.
Public Property RoundEnabledSpecifies whether rounding is enabled.
Public Property RoundRadiusSpecifies the radius of the round.
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TransformsReturns a read-only variant.
Public Property TypeSpecifies the type of the object being referenced.
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

MountingBoss Object