Solid Edge Part Type Library
Status Property
Description
Returns the status of the specified object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Status( _
   Optional ByRef Description As Variant _
) As FeatureStatusConstants
Parameters
Description
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objModel As SolidEdgePart.Model
    Dim objPatternPlane As SolidEdgePart.RefPlane
    Dim objFeatArray(1 To 2) As Object
    Dim objProfile As SolidEdgePart.Profile
    Dim objRPatterns As SolidEdgeFrameworkSupport.RectangularPatterns2d
    Dim objRPattern As SolidEdgeFrameworkSupport.RectangularPattern2d
    Dim objPattern As SolidEdgePart.Pattern
    Dim cStaus As SolidEdgeConstants.FeatureStatusConstants
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create base model for patterning
    If CreateModel(objDoc) <> "" Then
        MsgBox "Error in creating the base model"
        Exit Sub
    End If
    Set objModel = objDoc.Models(1)
    '***** Create a Rectangular Pattern of SmartPattern Type
    ' Create a new Profile object
    Set objPatternPlane = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objDoc.RefPlanes(1), _
                                                                 Distance:=0.025, normalside:=igRight, local:=True)
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(objPatternPlane)
    ' Get the RectangularPatterns2d object on the Profile
    Set objRPatterns = objProfile.RectangularPatterns2d
    ' Add an item to the RectangularPatterns2d collection
    Set objRPattern = objRPatterns.Add(OriginX:=-0.035, OriginY:=-0.035, _
                                       Width:=0.1, Height:=0.075, Angle:=0, OffsetType:=sePatternFillOffset, _
                                       XCount:=1, YCount:=1, XSpace:=0.025, YSpace:=0.025)
    Set objFeatArray(1) = objModel.ExtrudedProtrusions(2)
    Set objPattern = objModel.Patterns.Add(NumberOfFeatures:=1, _
                                           FeatureArray:=objFeatArray, Profile:=objProfile, PatternType:=seSmartPattern)
    objProfile.Visible = False
    ' Get the status of the Feature
    cStaus = objPattern.Status
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objModel = Nothing
    Set objPatternPlane = Nothing
    Set objFeatArray(1) = Nothing
    Set objFeatArray(2) = Nothing
    Set objProfile = Nothing
    Set objRPatterns = Nothing
    Set objRPattern = Nothing
    Set objPattern = Nothing
End Sub
See Also

Pattern Object  | Pattern Members