Solid Edge Part Type Library
Count Property
Description
Returns the number of objects in the referenced collection.
Property type
Read-only property
Syntax
Visual Basic
Public Property Count As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfileSets As SolidEdgePart.ProfileSets
    Dim lngCnt As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create two ProfileSet objects
    Set objProfileSets = objDoc.ProfileSets
    Call objProfileSets.Add
    Call objProfileSets.Add
    ' Get the Count property
    lngCnt = objProfileSets.Count
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfileSets = Nothing
End Sub
See Also

ProfileSets Collection  | ProfileSets Members