Solid Edge Part Type Library
Item Method
Variant (input) index.
Description
The items in a collection.
Syntax
Visual Basic
Public Function Item( _
   ByVal Index As Variant _
) As ProfileSet
Parameters
Index
Variant (input) index.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfileSets As SolidEdgePart.ProfileSets
    Dim objProfileSet1 As SolidEdgePart.ProfileSet
    Dim objProfileSet2 As SolidEdgePart.ProfileSet
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create a ProfileSet object
    Set objProfileSets = objDoc.ProfileSets
    Set objProfileSet1 = objProfileSets.Add
    ' Assign the ProfileSet object to the another object
    Set objProfileSet2 = objProfileSets.Item(1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfileSets = Nothing
    Set objProfileSet1 = Nothing
    Set objProfileSet2 = Nothing
End Sub
See Also

ProfileSets Collection  | ProfileSets Members