Solid Edge Part Type Library
Profiles Property
Description
Returns the Profiles collection object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Profiles As Profiles
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfileSet As SolidEdgePart.ProfileSet
    Dim objProfiles As SolidEdgePart.Profiles
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create a ProfileSet object
    Set objProfileSet = objDoc.ProfileSets.Add
    'Create a Profiles collection object
    Set objProfiles = objProfileSet.Profiles
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfileSet = Nothing
    Set objProfiles = Nothing
End Sub
See Also

ProfileSet Object  | ProfileSet Members