Solid Edge Part Type Library
RedefineFace Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method DropParentsRemoves associative connection with parents, so that it can not edited or recomputed.
Public Method ExactRange
Public Method GetEdgeTangencyTypesGet the edges input for redefine surface and its corresponding tangency types.
Public Method GetStatusExReturns the status of the specified object.
Public Method InsertSketchMethod to insert a sketch on a particular plane.
Public Method InsertUVCurveMethod to insert a key point curve representing U or V curve of a face at given parameter.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReorderInserts the referenced object in front of or behind another feature.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Method SetEdgeTangencyTypesSet specific tangency types on redefine surface edges.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DisplayName
Public Property EdgebarName
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property FaceMergeOptionGet set property for deciding which option to be used for Face merging.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property ReplaceFacesOnSolidBodyGet set property to decide if old faces should be replaced by newly created surface.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemName
Public Property TypeSpecifies the type of the object being referenced.
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

RedefineFace Object