Solid Edge Part Type Library
GetNormal Method
Returns the array of unit-vectors that are normal to the reference plane.
Description
Returns unit ectors that are normal to the surface at a specified point.
Syntax
Visual Basic
Public Sub GetNormal( _
   ByRef Normal() As Double _
) 
Parameters
Normal
Returns the array of unit-vectors that are normal to the reference plane.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objPPlane As SolidEdgePart.RefPlane
    Dim objRPParallel As SolidEdgePart.RefPlane
    Dim dblNormalVector() As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' geting the reference plane object
    Set objPPlane = objDoc.RefPlanes.Item(Index:=2)
    ' adding a reference plane parallel to and at a distance to a pricipal plane
    Set objRPParallel = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objPPlane, Distance:=0.01, _
                                                               NormalSide:=igLeft)
    ' Getting Normal vector to the reference plane
    Call objRPParallel.GetNormal(Normal:=dblNormalVector)

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPPlane = Nothing
    Set objRPParallel = Nothing
End Sub
See Also

RefPlane Object  | RefPlane Members