Solid Edge Part Type Library
Name Property
Description
Returns the name of the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Name As String
Remarks
All objects have names that are unique within the scope of their parent.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objPPlane As SolidEdgePart.RefPlane
    Dim objRPParallel As SolidEdgePart.RefPlane
    Dim strName As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Geting the reference plane object
    Set objPPlane = objDoc.RefPlanes.Item(Index:=2)
    'In V6 only Global RefPlanes are being named. To create a Global RP,
    'we should set the Local argument of the Add method to False.
    ' Adding a reference plane parallel to and at a distance to a pricipal plane and setting local argument to FALSE
    Set objRPParallel = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objPPlane, Distance:=0.01, _
                                                               NormalSide:=igLeft, Local:=False)
    ' getting the name of the reference plane
    strName = objRPParallel.Name
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPPlane = Nothing
    Set objRPParallel = Nothing
End Sub
See Also

RefPlane Object  | RefPlane Members