Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objModel As SolidEdgePart.Model
Dim objProfArr(1 To 2) As SolidEdgePart.Profile
Dim objLines As SolidEdgeFrameworkSupport.Lines2d
Dim objRelns1 As SolidEdgeFrameworkSupport.Relations2d
Dim objRelns2 As SolidEdgeFrameworkSupport.Relations2d
Dim objRefPln1 As SolidEdgePart.RefPlane
Dim objRefPln2 As SolidEdgePart.RefPlane
Dim objCutProf As SolidEdgePart.Profile
Dim objCutLines As SolidEdgeFrameworkSupport.Lines2d
Dim objExtCut As SolidEdgePart.ExtrudedCutout
Dim objRibs As SolidEdgePart.Ribs
Dim lngStatus As Long
Dim lngCnt As Long
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
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Draw the Profile
Set objProfArr(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
Set objLines = objProfArr(1).Lines2d
Call objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.04, y2:=0)
Call objLines.AddBy2Points(x1:=0.04, y1:=0, x2:=0.04, y2:=0.04)
Call objLines.AddBy2Points(x1:=0.04, y1:=0.04, x2:=0, y2:=0.04)
Call objLines.AddBy2Points(x1:=0, y1:=0.04, x2:=0, y2:=0)
' Relate the Lines to make the Profile closed
Set objRelns1 = objProfArr(1).Relations2d
Call objRelns1.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart)
Call objRelns1.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart)
Call objRelns1.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart)
Call objRelns1.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart)
' Check for the Profile Validity
lngStatus = objProfArr(1).End(igProfileClosed)
If lngStatus <> 0 Then
MsgBox ("Profile not closed")
End If
' Create the Base Protrusion Object
Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberofProfiles:=1, ProfileArray:=objProfArr, _
ProfilePlaneSide:=igRight, ExtrusionDistance:=0.04)
objProfArr(1).Visible = False
' Check the status of Base Feature
If objModel.ExtrudedProtrusions(1).Status <> igFeatureOK Then
MsgBox ("Error in the Creation of Base Protrusion Feature object")
End If
' Create a Cutout object Profile
Set objRefPln1 = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objDoc.RefPlanes(3), Distance:=0, NormalSide:=igRight)
Set objCutProf = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objRefPln1)
Set objCutLines = objCutProf.Lines2d
Call objCutLines.AddBy2Points(x1:=0.01, y1:=0.01, x2:=0.03, y2:=0.01)
Call objCutLines.AddBy2Points(x1:=0.03, y1:=0.01, x2:=0.03, y2:=0.03)
Call objCutLines.AddBy2Points(x1:=0.03, y1:=0.03, x2:=0.01, y2:=0.03)
Call objCutLines.AddBy2Points(x1:=0.01, y1:=0.03, x2:=0.01, y2:=0.01)
' Relate the Lines to make the Profile closed
Set objRelns2 = objCutProf.Relations2d
Call objRelns2.AddKeypoint(Object1:=objCutLines(1), Index1:=igLineEnd, Object2:=objCutLines(2), Index2:=igLineStart)
Call objRelns2.AddKeypoint(Object1:=objCutLines(2), Index1:=igLineEnd, Object2:=objCutLines(3), Index2:=igLineStart)
Call objRelns2.AddKeypoint(Object1:=objCutLines(3), Index1:=igLineEnd, Object2:=objCutLines(4), Index2:=igLineStart)
Call objRelns2.AddKeypoint(Object1:=objCutLines(4), Index1:=igLineEnd, Object2:=objCutLines(1), Index2:=igLineStart)
' Check for the Profile Validity
lngStatus = objCutProf.End(igProfileClosed)
If lngStatus <> 0 Then
MsgBox ("Profile not closed")
End If
' Create a Cutout object
Set objExtCut = objModel.ExtrudedCutouts.AddFinite(Profile:=objCutProf, ProfileSide:=igLeft, ProfilePlaneSide:=igLeft, Depth:=0.02)
objCutProf.Visible = False
' Check the status of CutOut Feature
If objModel.ExtrudedCutouts(1).Status <> igFeatureOK Then
MsgBox ("Error in the Creation of Cutout Feature object")
End If
' Create a Line object Profile for the Rib Feature
Set objRefPln2 = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objDoc.RefPlanes(3), Distance:=0.01, NormalSide:=igLeft)
Set objProfArr(2) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objRefPln2)
Call objProfArr(2).Lines2d.AddBy2Points(x1:=0.02, y1:=0.02, x2:=0.025, y2:=0.025)
' Create a Ribs collection object
Set objRibs = objModel.Ribs
' Create a Rib object
Call objRibs.Add(RibProfile:=objProfArr(2), ProfileExtensionType:=igExtend, _
ThicknessType:=igThkNormalToProfilePlane, _
MaterialSide:=igRight, ThicknessSide:=igRight, _
Thickness:=0.002)
objProfArr(2).Visible = False
' Check the status of Rib Feature
If objModel.Ribs(1).Status <> igFeatureOK Then
MsgBox ("Fails with options:- ProfileExtensionType:= igExtend, ThicknessType:=igThkNormalToProfilePlane, MaterialSide:=igRight, ThicknessSide:=igRight")
End If
' Get the Count Property of Ribs object
lngCnt = objRibs.Count
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objProfArr(1) = Nothing
Set objProfArr(2) = Nothing
Set objModel = Nothing
Set objLines = Nothing
Set objRelns1 = Nothing
Set objRelns2 = Nothing
Set objRefPln1 = Nothing
Set objRefPln2 = Nothing
Set objCutProf = Nothing
Set objCutLines = Nothing
Set objExtCut = Nothing
Set objRibs = Nothing
End Sub