| Solid Edge Part Type Library : RuledSurface Object |
AlterFacesForRuledSurface | Ruled Surface Alter Faces |
Delete | Deletes the referenced object. |
DropParents | Removes associative connection with parents, so that it can not edited or recomputed. |
ExactRange | |
GetRuledSurfaceEdges | Ruled Surface Edges |
GetStatusEx | Returns the status of the specified object. |
GetStyle | Returns the feature style. |
Range | Returns the high and low range values for the referenced object. |
Reorder | Inserts the referenced object in front of or behind another feature. |
RollToFeature | Rolls the referenced Model object back to a specified feature. |
SetRuledSurfaceEdges | Ruled Surface Edges |
SetStyle | Sets the feature style. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DisplayName | |
EdgebarName | |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
ModelingModeType | |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
RuledSurfaceAngle | Ruled Surface angle |
RuledSurfaceDirection | Ruled Surface direction |
RuledSurfaceDistance | Ruled Surface distance |
RuledSurfacePlaneOrAxis | Ruled Surface plane Or axis |
RuledSurfaceSide | Ruled Surface Side |
RuledSurfaceType | Ruled Surface type |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |