Solid Edge Part Type Library
AreCurvesValid Method
Specifies the number of elements in CurvesArray.
Specifies the Curve objects to be split.
Description
Verifies that the input curves for the referenced SplitCurves collection are construction curves.
Syntax
Visual Basic
Public Function AreCurvesValid( _
   ByVal NumberOfCurves As Long, _
   ByRef CurvesArray() As Object _
) As Boolean
Parameters
NumberOfCurves
Specifies the number of elements in CurvesArray.
CurvesArray
Specifies the Curve objects to be split.
See Also

SplitCurves Collection  | SplitCurves Members