Solid Edge Part Type Library
FacesByRay Property
Description
Returns a collection of faces that are intersected by a specified vector.
Property type
Read-only property
Syntax
Visual Basic
Public Property FacesByRay( _
   ByVal Xorigin As Double, _
   ByVal Yorigin As Double, _
   ByVal Zorigin As Double, _
   ByVal Xdir As Double, _
   ByVal Ydir As Double, _
   ByVal Zdir As Double _
) As Object
Parameters
Xorigin
Yorigin
Zorigin
Xdir
Ydir
Zdir
Remarks
The result of the FacesByRay property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used.
See Also

Unbend Object  | Unbend Members