Solid Edge Part Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objModel As SolidEdgePart.Model
    Dim objApplication As SolidEdgeFramework.Application
    Dim objUDPats As SolidEdgePart.UserDefinedPatterns
    Dim objProfiles As SolidEdgePart.Profiles
    Dim objProfile(1 To 2) As SolidEdgePart.Profile
    Dim objLines As SolidEdgeframeworkSupport.Lines2d
    Dim objRelns As SolidEdgeframeworkSupport.Relations2d
    Dim lngStatus As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Draw the Base Profile
    Set objProfile(1) = objDoc.ProfileSets.Add.Profiles.Add(objDoc.RefPlanes(3))
    Set objLines = objProfile(1).Lines2d
    Call objLines.AddBy2Points(X1:=0, Y1:=0, X2:=0.08, Y2:=0)
    Call objLines.AddBy2Points(X1:=0.08, Y1:=0, X2:=0.08, Y2:=0.06)
    Call objLines.AddBy2Points(X1:=0.08, Y1:=0.06, X2:=0.064, Y2:=0.06)
    Call objLines.AddBy2Points(X1:=0.064, Y1:=0.06, X2:=0.064, Y2:=0.02)
    Call objLines.AddBy2Points(X1:=0.064, Y1:=0.02, X2:=0.048, Y2:=0.02)
    Call objLines.AddBy2Points(X1:=0.048, Y1:=0.02, X2:=0.048, Y2:=0.06)
    Call objLines.AddBy2Points(X1:=0.048, Y1:=0.06, X2:=0.032, Y2:=0.06)
    Call objLines.AddBy2Points(X1:=0.032, Y1:=0.06, X2:=0.032, Y2:=0.02)
    Call objLines.AddBy2Points(X1:=0.032, Y1:=0.02, X2:=0.016, Y2:=0.02)
    Call objLines.AddBy2Points(X1:=0.016, Y1:=0.02, X2:=0.016, Y2:=0.06)
    Call objLines.AddBy2Points(X1:=0.016, Y1:=0.06, X2:=0, Y2:=0.06)
    Call objLines.AddBy2Points(X1:=0, Y1:=0.06, X2:=0, Y2:=0)
    ' Define Relations among the Line objects to make the Profile closed
    Set objRelns = objProfile(1).Relations2d
    Call objRelns.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(5), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(5), Index1:=igLineEnd, Object2:=objLines(6), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(6), Index1:=igLineEnd, Object2:=objLines(7), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(7), Index1:=igLineEnd, Object2:=objLines(8), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(8), Index1:=igLineEnd, Object2:=objLines(9), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(9), Index1:=igLineEnd, Object2:=objLines(10), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(10), Index1:=igLineEnd, Object2:=objLines(11), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(11), Index1:=igLineEnd, Object2:=objLines(12), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(12), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart)
    ' Check for the Profile Validity
    lngStatus = objProfile(1).End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Profile not closed")
    End If
    'Create the Base Extruded Protrusion Feature
    Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
                                                             profileArray:=objProfile, profileplaneSide:= _
                                                             igRight, ExtrusionDistance:=0.05)
    objProfile(1).Visible = False
    ' Check the status of Base Feature
    If objModel.ExtrudedProtrusions(1).Status <> igFeatureOK Then
        MsgBox ("Error in the Creation of Base Protrusion Feature object")
    End If

    ' Create a UserDefinedPattern Collection object
    Set objUDPats = objModel.UserDefinedPatterns
    ' Get the Application Property of UserDefinedPatterns object
    Set objApplication = objUDPats.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objApplication = Nothing
    Set objUDPats = Nothing
    Set objProfiles = Nothing
    Set objProfile(1) = Nothing
    Set objLines = Nothing
    Set objModel = Nothing
    Set objRelns = Nothing
End Sub
See Also

UserDefinedPatterns Collection  | UserDefinedPatterns Members